AXIS#.VL.KIWAITFORSETTLE

Description

AXIS#.VL.KIWAITFORSETTLE allows you to configure when the integrator will turn on and off based on current motion conditions. See AXIS#.MOTIONSTAT.SETTLED for more details on how to configure settling criteria.

Value Description
0 Integrator is always active
1 Integrator is active when AXIS#.MOTIONSTAT.SETTLED is 1
2 Integrator is active when AXIS#.MOTIONSTAT.SETTLED is 0

Versions

Action Version Notes
Implemented 02-13-01-000  
Modified 02-14-02-000 Mode 2 added

General Information

Type

Read/Write
Description Activates the velocity integrator only when the axis has settled.

Units

N/A

Range

0 – 2

Default Value

0

Data Type

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.KIWAITFORSETTLE

5011h

28h

Unsigned8

-

-

Read/Write

No

AXIS2.VL.KIWAITFORSETTLE

5111h

28h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6045

1

6045 (0x179d)

AXIS1.VL.KIWAITFORSETTLE

Unsigned8

Read/Write

Yes

71581

2

6045 (0x179d)

AXIS2.VL.KIWAITFORSETTLE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KIWAITFORSETTLE

6045

Unsigned8

Read/Write

-